Create a label that shows the current user

Create a label that shows the current user

Persistently indicate the currently logged in user.
SUGGERIMENTO: You can use the preconfigured label instead of creating it from scratch. For more information, select
Template Libraries
and select
Widgets
Username Label
.
  1. Right-click
    MainWindow (type)
    and select
    New
    Base controls
    Label
    .
  2. Hover over the label, select
    Edit
    , then type
    LabelCurrentUser
    .
  3. In the
    Properties
    pane, create a dynamic link between the
    Text
    property and
    Aliases
    {Session}
    Session
    User (Pointer)
    User (Pointed)
    .
    For more information about dynamic links, see Create dynamic links.
Fornire un feedback
Hai domande o feedback su questa documentazione? invia il tuo feedback qui.
Normal