Add retentivity storage to the project
Add retentivity storage to the project to make changes persistent.
- InProject view, right-clickRetentivityand select .
- InProperties, next toNodes, select.
- Create a dynamic link betweenNode1and .For more information about dynamic links, see Create dynamic links.
Fornire un feedback