Create a database
You need to add table to the data store before you start querying it.
- InProject view, right-clickDataStoresand selectEmbedded databaseorODBC database.
- InProperties, next toTablesselect.
- Add three table columns of Int16, Int32, and Float data types:
- Under the created table, next toColumnsselect.
- Next to the column, selectBaseDataTypeand selectInt16.
- Next toColumns, select.
- Next to the column, selectBaseDataTypeand selectInt32.
- Next toColumnsselect.
- Next to the column, selectBaseDataTypeand selectFloat.
Fornire un feedback