IUAVariable.SetDynamicLink(source, sourceArrayIndex, mode)

Sets a dynamic link to a specific array (first argument) cell (second argument). The third argument is optional and sets the dynamic link mode.
void SetDynamicLink(IUAVariable
source
, uint
sourceArrayIndex
, DynamicLinkMode
mode
);

Arguments

source
(IUAVariable)
The
BrowseName
of the source variable.
sourceArrayIndex
(uint)
A cell of the source array.
mode
(DynamicLinkMode)
An optional argument that specifies the dynamic link mode.
The following dynamic link modes are available:
DynamicLinkMode.Read
(default)
Read (from source node to parent).
DynamicLinkMode.Write
Write (from parent to source).
DynamicLinkMode.ReadWrite
Read and write (bidirectional).
ResourceURI
A C# object that contains the path indicated in the argument.

Example

The following example shows an API that sets a read dynamic link on the
Speed
property (whose node is represented by
SpeedVariable
) of the
Motor1
object. The link source is the second cell of the
SpeedList
array:
var myObj = Owner.Get<Motor>("Motor1"); var speedValue = Project.Current.FindVariable("SpeedList"); myObj.SpeedVariable.SetDynamicLink(speedValue, 2, DynamicLinkMode.Read);
Fornire un feedback
Hai domande o feedback su questa documentazione? invia il tuo feedback qui.