IUANode.FindVariable(browseName)

Returns an
IUAVariable
C# object. The returned object corresponds to the first child variable found in the node children on which the method is invoked. The returned object name corresponds to the argument.
IUAVariable FindVariable(string
browseName
);

Arguments

browseName
(string)
The
BrowseName
of the node to find.

Returns

IUANode
A C# object that corresponds to the variable found.

Example

The following example shows a returned C# object that corresponds to the first
Speed
variable child of the project root node:
var currentSpeed = Project.Current.FindVariable("Speed");
Fornire un feedback
Hai domande o feedback su questa documentazione? invia il tuo feedback qui.