IUANode.ChildrenRemoteRead(timeoutMilliseconds)
Returns the list of all the direct child variables of the node on which it invokes. The optional argument sets the timeout period.
IEnumerable<RemoteChildVariableValue> ChildrenRemoteRead(doubletimeoutMilliseconds);
Arguments
- timeoutMilliseconds(double)
- The timeout period, expressed in milliseconds, after which the API throws an exception.MANCIA: If not specified, the default value of the argument is30000(30 seconds).
Returns
- IEnumerable<RemoteChildVariableValue>
- The list of direct child variables of the node, expressed as a pair of theRemoteChildVariableValueclass following properties:
- RelativePath(string)
- The path relative to the variable inside the node.
- Value(UAValue)
- The value of the variable.
Example
The following example shows an API that returns the
reads
list of all the variables contained in the myNode
node. For each variable (item
), a message is generated that shows the relative path and value.If the API returns an error or if the set timeout time is reached, the code in the following example generates an error message composed of
and an expected error code for the API.ChildrenRemoteRead failed:
var myNode = Project.Current.Get("CommDrivers/Driver1/Station1/Tags/TagStructure1"); try { var reads = myNode.ChildrenRemoteRead(); foreach (var item in reads) Log.Info("Tag " + item.RelativePath + " has value " + item.Value); } catch (Exception ex) { Log.Error("ChildrenRemoteRead failed: " + ex.ToString()); }
Fornire un feedback