ResourceURI.FromAbsolutePath(path)
Returns a C# object of the
ResourceURI
type, with the URIType
of AbsoluteFilePath
that contains an absolute path to a file.static ResourceUri FromAbsoluteFilePath(stringpath);
Arguments
- path(string)
- An absolute path to a file.
Returns
- ResourceURI
- A C# object that contains the path indicated in the argument.
Example
The following example shows an API that returns a C#
applicationRelativeResourceURI
object of theResourceURI
type that contains the relative path C:\Users\Username\Desktop\Text1.txt
.var applicationRelativeResourceUri = ResourceUri.FromAbsolutePath("C:\Users\Username\Desktop\Text1.txt");
Fornire un feedback