Session activity log and audit

The C# APIs are supplied by the
Session
C# class and displayed by NetLogic, which represents the session in which the instance of NetLogic at runtime exists.
Fornire un feedback
Hai domande o feedback su questa documentazione? invia il tuo feedback qui.