Develop a user management interface

Develop a multilingual user management solution.
MANCIA: Instead of creating the user management interface from scratch, you can use the predefined widgets. For more information, from the toolbar, select Template Libraries and search for
User Editor
The user management interface enables you to:
  • Create user accounts
  • Remove user accounts
  • Change the password and location of user accounts
Application example
MANCIA:
You can download a sample project from:
ExampleApplication-UserManagementInterface.zip
Prerequisites:
In
FactoryTalk Optix Studio
, select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Fornire un feedback
Hai domande o feedback su questa documentazione? invia il tuo feedback qui.