Add the Zip Unzip NetLogic
The Zip Unzip NetLogic enables you to compress and decompress files and folders.
Prerequisites:
Set the default external code editor. See Set the default code editor.
- From theFactoryTalk Optix Studiotoolbar, select .
- In theLibrarieswindow, in the top list, selectScripts.
- From theComponentslist, dragZip Unziponto theMainWindow (type)inProject view. SelectClose.
- Add the NuGet Gallery | SharpZipLib package. SeeAdd NuGet packages.
The Zip Unzip NetLogic is added to your project. The NetLogic exposes the
CreateZipArchive
and UnzipArchive
methods. For reference, see zipunzip-netlogic.Fornire un feedback