Configure the amount of information in the Output pane
The module log level configuration specifies the maximum level of information displayed in the
Output
panel. By default, the FactoryTalk Optix Studio
Output
pane shows warnings and all errors of maximum and minimum severity. All information is stored in the system log file, regardless of the maximum information level displayed in FactoryTalk Optix Studio
.Change the level of information displayed in the
Output
panel for all FactoryTalk Optix Studio
Platform modules or just specific modules.- In the main toolbar, selectFactoryTalk Optix Studio Options.
- SelectAdvanced mode, and then selectClose.
- CloseFactoryTalk Optix Studioand then reopen the software to enable the updated options settings to take effect.
- Select the down arrow onFactoryTalk Optix Studio Optionsand selectModule log level configuration.Module log level configurationopens and lists every module in the project.
- Set the information level:
- InDefault level, select the default maximum information level for messages generated by all modules.
- (optional) For each individual module, override the default level with a specific information level for that module.
- SelectClose.
Fornire un feedback