- Manuale introduttivo
- Utilizzo del software
- OPC UA
- Oggetti grafici e di layout
- Sessioni e impostazioni locali
- Sviluppo di soluzioni
- Sviluppo di progetti con C#
- NetLogic
- Metodi ed eventi in C#
- Riferimento API C#
- Esempi di applicazione
- Esercitazione dell'interfaccia utente
- Esercitazione sui collegamenti dinamici
- Esercitazione sui logger
- Esercitazione sugli allarmi
- Esercitazione sulle NetLogic
- Riferimento su oggetti e variabili
Main toolbar
The main toolbar at the top of the user interface contains buttons that all views use.
Item | Description | Function |
---|---|---|
![]() | Close project | Closes the current project. |
![]() | Save | Saves the project. Select an option from the list to:
|
![]() | Save and Commit | Save changes and commit the changes to back them up in the local repository. |
![]() | Push to remote | Push saved and committed changes to the remote repository for users to see the latest changes to the project. |
![]() | Pull from remote | Pull the latest changes from the remote repository to see the latest changes that other users have made. |
![]() | View History | View the history of changes to the project. Restore any commit to revert to a previous version of the project. |
![]() | Undo | Cancels the last operation. |
![]() | Redo | Repeats the last operation. |
![]() | Browse project files | Opens the project resource window for displaying, importing, or deleting project files such as, images, videos, documents, and certificates. |
![]() | Template Libraries | Opens the default and custom libraries and template variables. |
![]() | Open .NET Solution | Opens the .NET project to incorporate additional functionality using custom C# code. |
![]() | Open dashboard page | Opens a configuration dashboard to begin designing your user interface. Select the list to configure the connected device, data logging, and recipes, or manage users and groups. |
![]() | Stop | Stops the application that is running on the client device. |
![]() | Run on Emulator | Compiles, transfers, and runs the application on the selected client device or emulator. Select a different client device from the list. . |
Fornire un feedback