Start page
The Start page opens when you launch
FactoryTalk Optix Studio
. It appears for you to create or open a project before you see the FactoryTalk Optix Studio
interface.The Start page allows you to open and create projects using three views:
Home
Create a
Default
project that contains all Project view
categories and a preconfigured main window or create a Blank
project that has no predefined content. You can search for a recent project or filter projects to see local or remote projects.New
Create a
Default
project that contains all Project view
categories and a preconfigured main window or create a Blank
project that has no predefined content. When creating a new project, use version control to be able to open a version of the project that contains specific changes. Open
Open a recent or remote project. When opening a remote project, enter a
Remote URL
to clone a repository and create a project with the same name as the repository, or enter a Location
to open an existing project in the remote repository. Fornire un feedback