Change the user authentication mode

Change the user authentication mode

Change the default user authentication mode to allow local
Windows®
users and Active Directory users to log into the
FactoryTalk Optix Application
.
  1. In the
    Project view
    pane, select
    ProjectName
    .
  2. In the
    Properties
    pane, set the
    Authentication mode
    .
    • Model only
      . Allows only the users created in
      FactoryTalk Optix Studio
      to log in.
    • Local only
      . Allows only local
      Windows
      users to log in.
    • Active Directory
      . Allows only Active Directory users to log in.
    • Domain Only
      . Allows only Active Directory users and local
      Windows
      users to log in.
    • Any
      . Allows users of any type to log in.
    For more information, see AuthenticationMode.
Fornire un feedback
Hai domande o feedback su questa documentazione? invia il tuo feedback qui.
Normal