DENSO Robotics
Company Overview
As one of the world's largest automotive parts manufacturers, DENSO is also the world's largest manufacturer of small assembly robots. DENSO offers a wide range of compact 4-axis SCARA and 5- and 6-axis articulated robots, for payloads up to 20 kg and reaches from 350 to 1,300 mm.
Expertise/Offerings
Industries
- Food & Beverage
- Life Sciences
Product Categories
- Robotics
Partner Highlights
產品
產品 | Product Category | 說明 |
---|---|---|
RC8 Robot Controller | Robotics | Robot controller with EtherNet/IP allows users to program a DENSO robot from a ControlLogix/CompactLogix. |
Participating Regions
北美
Latin America
EMEA
Asia Pacific
DISCLAIMER: Please note that the information herein is provided to Rockwell Automation by the partner and has not been validated by Rockwell Automation. It is intended to provide general commercial information and you should not rely on it before making any purchasing or technical decision. ROCKWELL AUTOMATION DOES NOT WARRANT THE COMPLETENESS, TIMELINESS, OR ACCURACY OF ANY OF THE INFORMATION HEREIN, NOR ASSUME ANY LIABILITY, AND MAY MAKE THERETO CHANGES AT ANY TIME IN ITS SOLE DISCRETION WITHOUT NOTICE. Rockwell Automation also does not assume any liability over the solution or work provided by its partners.