Configure an application as an MQTT client

Configure an application as an MQTT client

Message Queue Telemetry Transport (MQTT) is a standard ISO protocol based on a message broker, which is responsible for distributing messages to recipient clients.
Application example
SUGGERIMENTO:
You can download a sample project from:
ExampleApplication-MQTTClient.zip
Prerequisites:
In
FactoryTalk Optix Studio
, select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Fornire un feedback
Hai domande o feedback su questa documentazione? invia il tuo feedback qui.
Normal