Configure the message broker IP

You set the IP address for the message broker by creating a variable.
  1. In the
    Project view
    pane, right-click the
    Model
    folder and select
    New
    Variable
    .
  2. In the
    Project view
    pane, hover-over the variable, select 
    Edit
    , and enter
    BrokerIpAddress
    .
  3. In the
    Properties
    pane, select
    Int32
    and select
    String
    .
  4. In the
    BrokerIpAddress
    property value, enter the IP address of the MQTT broker.
    For testing purposes, you can enter
    test.mosquitto.org
Fornire un feedback
Hai domande o feedback su questa documentazione? invia il tuo feedback qui.