Semi Circle Pie Chart

  1. Open a Storyboard, hover the mouse on a chart tile and click the [] icon to maximize the tile.
  2. Click the [] icon. The Chart Settings window displays.
    View
    Under the Type tab, the list of available chart types display.
  3. Click [Pie Chart]. The available chart models display.
  4. Select the [Semi Circle] chart from the Pie Chart section.
    Chart Settings
  5. Under the Configuration tab, provide the following properties:
    • Y-Axis: Select the desired attribute using the [] icon. User can add more than one Y-Axis values for this chart.
    • X-Axis: Select an attribute of date type.
      NOTE:
      Multiple X-Axis values are not allowed for this chart type.
    • Legend: Select a desired field from the drop-down list to apply a different series on top of X-Axis or Y-Axis for comparing the available data.
    • Tooltip: User can select the values to be displayed on the tooltip.
  6. Click [Apply].
    The Semi Circle Pie Chart displays.
    Semi Circle Pie Chart
  7. Click the [] icon to minimize the chart. The updated Storyboard displays.
    Storyboard Updated
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.