Pie Charts

Pie Charts

A Pie Chart is a circular chart divided into sectors which is proportional to the quantity it represents.
The Pie Charts are used to represent the proportional data or relative data in a single chart. The concept of pie slices is used to show the percentage of a particular data from the whole pie.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal