Configure an application as an MQTT client

Message Queue Telemetry Transport (MQTT) is a standard ISO protocol based on a message broker, which is responsible for distributing messages to recipient clients.
Application example
TIP:
You can download a sample project from:
MQTTClient.zip
Prerequisites
In
FactoryTalk Optix Studio
, select
Run
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.