Configure the message broker IP

You set the IP address for the message broker by creating a variable.
  1. In
    Project view
    , right-click the
    Model
    folder and select
    New
    Variable
    .
  2. In
    Project view
    , hover-over the variable, select
    Edit
    Edit
    , and enter
    BrokerIpAddress
    .
  3. In
    Properties
    , select
    Int32
    and select
    String
    .
  4. In the
    BrokerIpAddress
    property value, enter the IP address of the MQTT broker.
    For testing purposes, you can enter
    test.mosquitto.org
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.