Conversion Constant and Drive Resolution Attributes
The settings for certain axis attributes come from the settings of the Conversion Constant (set on the Conversion tab), or the Drive Resolution (set on the Drive tab).
When you edit the setting for either the Conversion Constant or the Drive Resolution, and then click either
OK
or Apply
, you must choose whether to also recalculate the settings for these dependent attributes.If you choose
Yes
, the controller recalculates the settings for the following attributes:On this tab or dialog: | These attributes are recalculated: |
Dynamics tab | Maximum Velocity Maximum Acceleration Maximum Deceleration |
Limits tab | Position Error Tolerance |
Custom Drive Scaling Attributes dialog | Torque Scaling |
Custom Limit Attributes dialog | Velocity Limit Bipolar Velocity Limit Positive Velocity Limit Negative Acceleration Limit Bipolar Acceleration Limit Positive Acceleration Limit Negative |
If you choose
No
, the settings for these attributes remain unchanged.Provide Feedback