Module Properties Dialog Box - Power Tab Overview (PowerFlex 700S and PowerFlex 700SE with DriveLogix5720, PowerFlex 700S 2 and PowerFlex 700Se2 with DriveLogix5730, PowerFlex/DPI, SCANPort)
When Interleave Interrupts is set Real Time Sample (RTS) period must be zero, Conversion Rate should be 1200 Hz and the Low Pass Time Constant should be none.