Modify Custom Language dialog box overview
Use the Modify Custom Language dialog box to reconfigure a custom language.
Parameter | Description |
---|---|
Old Name | Displays the current name for the custom language. |
Old Root Language | Displays the current root language that is associated with the custom language. |
New Name | Enter a unique name for the custom language following the RFC1766 naming conventions.
The following are RFC1766 naming conventions.
|
New Root Language | Select a root language to associate with the custom language. Root languages cannot be custom languages. If a root language is specified, the custom language appears along with the root language in lists such as the Localize To list in the export wizard. |
New Full Name | The custom language prefixed with the RFC1766 name of the specified root language. When a root language is not specified, the name is prefixed with x-. |
Provide Feedback