Real Time Sample too small
The work that the module does to:
module
A device, typically an I/O device, that communicates with the controller. The controller, a particular 1756-IB16I or a PanelView are all considered modules.
- sample the inputs
- linearize to temperature
- convert to floating point
- perform scaling
- check the various alarms
requires a higher RTS period.
If you are configuring: | Enter an RTS value that is: |
a non-isolated 1756-IF8, 1756-IF16 analog input module in float data - high speed mode | 8 ms or higher |
a 1756-IR6I or 1756 IT6I analog input module in floating point mode and a Sensor is specified | 50 ms or higher |
a module in integer mode | 10 ms or higher |
a module in floating point mode | 25 ms or higher |
The RTS indicates how often the modules’ inputs are to be sampled.
There is only one RTS for the entire module.
Provide Feedback