Rate Alarm too large
The current Rate Alarm setting is too large. Select a smaller Rate Alarm setting from the Alarm Configuration Tab.
The Rate Alarm value indicates to trigger when the rate of change between input samples exceeds the setpoint. Set this alarm in terms of Engineering Units/Second.
Provide Feedback