Download
After a program is created in Logix Designer it must be transferred from the computer to the controller.
- Upload - Transfers the program from the controller to the computer.
- Download - Transfers the program from the computer to the controller.
Performing this task uses these items:
Item | Description |
---|---|
Communications tree | A hierarchical representation of a network topology that is rooted at a specific server host device. |
Who Active | Who Active is a communication software edition network browser. Use the Who Active dialog box to navigate network topologies and configure access methods used to communicate with devices. Both the RSLinx Classic and FactoryTalk Linx communication software editions are included with Studio 5000 Logix Designer . Select an edition to launch in the Who Active dialog box by navigating to Communications > Select Communication Software dialog box and selecting RSLinx Classic or FactoryTalk Linx . |
Communication Path | This is the CIP path that identifies the communications drive, the device address, and port. It is used by Studio 5000 Logix Designer when executing a Go Online, Upload, or Download command. |
Program mode | The controller mode during which logic is not executing, outputs are not controlled, and editing operations are available. If the keyswitch is in Remote, the controller is in Remote Program mode. |
To download a program
- SelectCommunications >Who Active.The communication software launches in theWho Activedialog and displays the communications tree.
- Select a controller from the tree.
- SelectSet Project Pathto always use this communications path with this project.
- SelectDownload.Confirm the download procedure. Since the communications path is configured, the download works immediately, and the project is downloaded to the controller. Download status and compiler messages appear in the status bar.TIP:The controller must be in Program mode or Remote Program mode before downloading the project.
Provide Feedback