Generator Tab

Use this tab to record specific information from your generator. You can typically find this information on the generator’s nameplate.
Parameters
Frequency
Enter the generator’s rated frequency. Valid values are 50 Hz and 60 Hz (default).
Voltage
Enter the generator’s rated voltage. Valid values range from 85.0 V to 30,000 V. The default value is 480.0 V.
Current
Enter the generator’s rated current. Valid values range from 10.0 A to 60,000.0 A. The default value is 60.0 A.
Power
Enter the generator’s rated power. Valid values range from 0 W to 1,000,000,000.0 W. The default value is 300,000.0 W.
Field Voltage
Enter the generator’s rated field voltage. Valid values range from 1.0 V to 200.0 V. The default value is 75.0 V.
Field Current
Enter the generator’s rated field current. Valid values range from 0.1 to 15.0 A. The default value is 3.0 A.
OK
Click this button to accept your edits on any tab and close the dialog.
Cancel
Click this button to cancel your edits on any tab and close the dialog.
Apply
Click this button to apply your edits on any tab and continue editing.
Help
Click this button for help on this tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.