Check Out Dialog Box
Use this dialog box to retrieve a file.
Parameters
Parameter | Description |
---|---|
Comments | Enter a comment up to 255 characters in length. Comments longer than 255 characters are truncated. |
Retrieve a local copy | If not checked, AssetCentre marks the file as checked-out to the location shown in the To field, without actually downloading the file to that location. If checked, AssetCentre marks the file as checked-out and downloads the file to the location shown in the To field. |
To | Identifies the location for the checked out file. Type a new destination or select ellipses to choose a new destination for the file. |
Working Folder Browse button | Open the Browse for Folder dialog box to choose a folder to use as the working folder. |
OK | Start the file check out process (if you initiated this process from the Open/Import Project dialog box). If the specified directory in the To field does not exist, the Logix Designer application prompts to create the directory. If the directory is created, AssetCentre uses that directory as the working folder and continues with the check out operation. If the directory is not created, the Check Out dialog box appears. |
Cancel | Close the Check Out dialog box without completing the check out operation. |
Help | View help about the Check Out dialog box. |
Provide Feedback