File with same name exists
A writable instance of the file is open in another instance of the
Logix Designer
application. The file was not retrieved.Option | Description |
---|---|
OK | Return to the Open/Import Project dialog box. |
Help | View Help on this error. |
Provide Feedback