New Folder Dialog Box Overview

Use this dialog box to create a new folder within the source control database.
Parameters
Parameter
Description
Name
Enter the name of the new folder.
Comments
Enter a comment up to 255 characters in length. Comments longer than 255 characters are truncated.
OK
Create the new folder within source control.
Cancel
Return to the Add Project to Source Control dialog box without creating the new folder.
Help
Help on this dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.