Select Master Coordinated System Time
To select the master coordinated system time
- Right-click theControllerfolder.
- SelectProperties. TheController Propertieswindow appears.
- Select theDate/Timetab.If:And:Then:Your controller uses a motion axisNo other controllers in your chassis are configured as the master controller
- Select Make this controller the master
- Select OK
Your controller uses a motion axisAnother controller in your chassis is configured as the master controller- Select OK
Provide Feedback