Reference Information by Connection
The
By Connection
tab shows the cross references to the tag or module, specified in the Name
field, via connections. Each line represents a single connection between two endpoints. Use the By Connection
cross reference tab to view connections for the tag, parameter, members, module, or bit specified in the Name
field.Cross Reference information:
- Reference - Shows the connection endpoint for the selected tag or module.
- ->, <-, <->, ?
- Identifies the direction of the connection.
- -> the connection is from the tag.
- <- the connection is to the tag.
- <-> the connection is to and from the tag.
- ? the connection is not valid.
- Endpoint
- Identifies the connection endpoint. Use the direction arrows (->, <-, <->) to determine the direction of the connection to the endpoint (from the tag, to the tag, or to and from the tag). To view tags referenced by alias tags, click the By Tag tab in the Cross Reference window. TheBy Connectiontab shows only connections to or from the alias tag.
- Usage
- Shows the usage value for the tag listed in the Endpoint column.
To reference information by connection:
- Select the connection. TheTag Editorappears.
- Select browse in theConnectioncolumn of the connection to edit. TheConnection Configurationdialog box opens. Configure the connection's beginning endpoint.
Provide Feedback