Delete a tag

Delete a tag from the Tag Editor. Deleting a tag removes the tag from the program and throughout the project.
To delete a tag
  1. On the explorer bar, select System icon
    System
    .
  2. In
    System
    , right-click the program and select
    Tags and parameters
    .
  3. In the Tag Editor, select the row header cell of the tag to delete.
  4. Press
    Delete
    or right-click the selected row and select
    Delete
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.