Create a program

Use the
Create Program
dialog box to create programs for tasks and
FactoryTalk Smart Object
s. For large or complex programming tasks, it can help to break up the logic into multiple programs. Each program has its own tags that logic in other programs cannot access. You can create up to 1000 programs.
  1. On the explorer bar, select FTDStudioExecution
    Execution
    .
  2. Navigate to and right-click the item and select
    New Program
    .
  3. In
    New Program
    :
    • Name.
      Enter a name for the program.
    • Description.
      Enter a description of the program.
    • (Optional) Set
      Create a Main Routine
      to
      On
      .
    • Main Routine type.
      Select
      Ladder Diagram
      .
      • A Ladder Diagram is a specialized schematic to represent relay control logic.
  4. Select
    Create
    . The new program and main routine appear in FTDStudioSystemV1
    System
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.