Add a ladder diagram branch to a routine
Add a branch to a rung to indicate an OR operation. Instructions that you place in a branch instruct the routine to use either the instruction in the rung or the instruction in a branch or the instruction in a branch level or the next branch level.
Prerequisites
To add a ladder diagram branch to a routine
- From the Ladder EditorToolbox, drag a branch
to a valid drop zone in the rung. Valid drop zones are indicated by
.
TIP: IfToolboxis not visible, on the pane bar, selectToolbox. - (optional) Add an instruction or branch level to the branch.
Provide Feedback