Move a ladder diagram branch rail

Move ladder diagram branch rails to have the instructions on the branch execute at a different time in the routine.
Prerequisites
To move a ladder diagram branch rail
  • In the ladder diagram, drag the branch rail:
    • Left Branch Rail
      . Drag an operand of the left branch rail to move the entire branch level. This reorders the branch levels, places the level on another branch, or inserts the instructions on the branch level onto a rung.
    • Right Branch Rail
      . Drag a right branch rail to move the Right Branch Rail of the branch on the rung. When you move the right branch rail, dragging an end of the branch to the left or right to includes or excludes content.
      TIP: Valid drop zones are indicated by FTDStudioValidLDDropLocation.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.