Edit a ladder diagram rung

Edit a rung in a ladder diagram to change the functionality of the rung in the routine.
Prerequisites
To edit a ladder diagram rung
  1. From the main toolbar, select either FTDStudioSystemV1
    System
    or FTDStudioExecution
    Execution
    .
  2. Navigate to and double-click the routine. The editor opens the workspace of the routine.
  3. Select the rung to edit and make the necessary changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.