Add a ladder diagram rung to a routine
Add a rung to a routine so that you can add branches and instructions to the rung.
Prerequisites
To add a ladder diagram rung to a routine
- In the Ladder EditorToolbox, drag a rung
to the canvas of the routine. Valid drop zones are indicated by
.
TIP: IfToolboxis not visible, on the paneToolbox.
Provide Feedback