Search
Studio 5000 Logix Designer Online Help
P - Instruction Set
- P -
PAH
Process Analog Input (PAI)
Process Dual Sensor Analog Input (PAID)
Process Multi Sensor Analog Input (PAIM)
Process Analog Output (PAO)
PATT
Process Boolean Logic with Snapshot (PBL)
PCE
PCLF
PCMD
Process Command Source (PCMDSRC)
Process Discrete 2-, 3-, or 4-State Device (PD4SD)
Process Deadband Controller (PDBC)
PDET
Process Discrete Input (PDI)
Process Discrete Output (PDO)
Process Dosing (PDOSE)
PFL
Process Analog Fanout (PFO)
Process High or Low Selector (PHLS)
PI
PID
Enhanced PID (PIDE)
Process Interlocks (PINTLK)
Process Lead Lag Standby Motor Group (PLLS)
Process Motor (PMTR)
PMUL
Process n-Position Device (PNPOS)
Position Proportional (POSP)
POVR
PPD
Process Permissives (PPERM)
Process Proportional + Integral + Derivative (PPID)
Pressure/Temperature Compensated Flow (PPTC)
Process Restart Inhibit (PRI)
PRNP
Process Run Time and Start Counter (PRT)
PSC
Process Tank Strapping Table (PTST)
Process Valve (PVLV)
Process Mix Proof Valve (PVLVMP)
Process Valve Statistics Object (PVLVS)
Process Variable Speed Drive (PVSD)
PXRQ
Instruction Set
Provide Feedback
Have questions or feedback about this documentation? Please
submit your feedback here
.