PlantPAx instructions

The PlantPAx built-in instructions monitor and process discrete and analog inputs and outputs for controlling devices.
Available Instructions
Ladder Diagram, Function Block, Structured Text
To:
Use this instruction:
Provide HART digital data for an intelligent analog device alongside the analog input (PAI) or analog output (PAO) instruction for that device.
Process Analog HART (PAH)
Monitor one analog value, such as from a channel of analog input module.
Process Analog Input (PAI)
Monitor one analog Process Variable (PV) by using two analog input signals.
Process Dual Sensor Analog Input (PAID)
Monitors one analog process variable (PV) by using up to eight analog input signals.
Process Multi Sensor Analog Input (PAIM)
Manipulate an analog output to control a field device.
Process Analog Output (PAO)
Executes up to eight gates of configurable Boolean logic.
Process Boolean Logic (PBL)
Select the Command Source for a device.
Process Command Source (PCMDSRC)
Control and monitor feedback from a discrete 2-state, 3-state, or 4-state device in a variety of modes.
Process Discrete 2-, 3-, or 4-State Device (PD4SD)
Generate outputs to provide data and alarms on deadbands and thresholds.
Process Deadband Controller (PDBC)
Monitor one discrete condition, such as from a channel of a discrete input module.
Process Discrete Input (PDI)
Manipulate a discrete output to control a field device.
Process Discrete Output (PDO)
Control an ingredient addition that uses a flow meter to measure the quantity of ingredient added.
Process Dosing (PDOSE)
Send one primary analog output signal to multiple secondary users or devices.
Process Analog Fanout (PFO)
Select the highest or the lowest of up to six incoming controlled variables (CVs) and send the selected CV as output.
Process High or Low Selector (PHLS)
Collect, or sum up, the interlock conditions that stop or de-energize a running or energized piece of equipment.
Process Interlocks (PINTLK)
Control a parallel group of motors, such as a set of pumps with a common intake source and discharge destination.
Process Lead Lag Standby Motor Group (PLLS)
Monitor and control a fixed single-speed, two-speed, or reversing motor.
Process Motor (PMTR)
Control and monitor feedback from a circular or linear discrete device with up to 30 positions.
Process n-Position Device (PNPOS)
Collect, or sum up, the permissive conditions that allow a piece of equipment to energize.
Process Permissives (PPERM)
Manipulate the Control Variable (CV) in regulatory control loops in response to Process Variable (PV) readings and Setpoint (SP, the target PV) settings.
Process Proportional + Integral + Derivative (PPID)
Calculate a flow at standard temperature and pressure.
Process Pressure/Temperature Compensated Flow (PPTC)
Prevent large motors from starting repeatedly.
Process Restart Inhibit (PRI)
Record the total run time and number of instances the motor or other equipment starts.
Process Run Time and Start Counter (PRT)
Calculate the volume of product in an upright cylindrical tank, given the level of the product and the tank calibration table.
Process Tank Strapping Table (PTST)
Operate a two-position, single-solenoid operated valve, a dual-solenoid operated valve, or a motor-operated valve in various modes; monitor hand-operated two-position valves.
Process Valve (PVLV)
Control and monitor feedback from a mix-proof valve in various modes and states.
Process Mix Proof Valve (PVLVMP)
Monitor a two-state (open and close) valve and record statistics for stroke times and stroke counts.
Process Valve Statistics (PVLVS)
Monitor and control a variable-speed motor using an AC (variable frequency) or DC drive.
Process Variable Speed Drive (PVSD)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.