Apply animations to graphic objects

Apply animations to graphic objects

Add and configure number, sequential, or parallel animation properties to animate a graphic object.
  1. In
    Project view
    , select the graphic object to animate.
  2. In
    Properties
    , at the top, select
    Add
    and then select either:
    • Number animation
      .
    • Sequential animation
      .
    • Parallel animation
      .
    For more information, see Animations.
  3. Configure animation properties. See Animation properties.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal