DriveFault - Servo Drive
Applies to: Servo Drive axis.
DriveFault is a 32-bit attribute. Its value is set upon the occurrence of any of the following faults. Click a fault from the following list for information about that fault.
Bit # | Fault Name |
8 - 12 | Reserved |
28 - 31 | Reserved |
The occurrence of a DriveFault sets both the PhysicalAxisFault attribute, and bit #0 of the AxisFault attribute.
To clear a DriveFault, you must diagnose and clear the underlying fault. The following instructions can be used to clear both the underlying fault and the DriveFault.
To clear a DriveFault:
- Fault Reset (MAFR) instruction, to clear all motion faults for an axis.
- In the case of a shutdown, a Shutdown Reset (MASR) instruction, to return to an axis ready operating state.
- For a grouped axis: Motion Group Shutdown Reset (MGSR) instruction, to transition a group of axes from the shutdown operating state to the axis ready operating state.
Provide Feedback