Lock graphic objects protected with a password
Lock a password-protected graphic object to prevent other
FactoryTalk Optix Studio
users from editing child objects of the protected object.- InProject viewor in theEditor, next to the object to lock, select .
In
Project view
and in the Editor
, appears next to the password protected object. The child objects are hidden in Project view
and cannot be edited.Provide Feedback