Unlock graphic objects protected with a password
Unlock a password protected graphic object to view and edit its child objects.
- InProject viewor in theEditor, next to the object to unlock, select .
- Enter the password and selectOK.
In
Project view
and in the Editor
, appears next to the password protected object. You can view and edit unlocked object child objects.Provide Feedback