Sequential Function Chart Editor

The
Sequential Function Chart Editor
is contained within the
Routine
window in the main
Logix Designer
application window. The editor provides a way to create and edit sequential function chart routines. The editor consists of tabs for all open routines, a view for each routine, and the Sequential Function Chart toolbar.
Use parameters in a routine from the current program or from another program.
Vertical and horizontal scroll bars appear in the
Sequential Function Chart Editor
when the current routine is too large to view in its entirety within the routine window. These scroll bars apply only to the routine currently in view.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.