Sequential Function Chart Routine Overview Dialog

The SFC Routine Overview dialog displays an overview, or bird's eye view, of the entire SFC routine in a pop-up window.
The zoom rectangle (red outline) indicates the portion of the routine that is currently displayed in the routine window, and as the zoom percentage. When moving and resizing the zoom rectangle, the main SFC editor window updates immediately to reflect the changes. Any active steps, actions, and stops are animated in the overview window.
Moving the cursor over an element shows the element's identifier, according to this format:
  • <cross reference grid location>, <element type>, <backing tag name>
    TIP:
    The backing tag name is not applicable to some elements, and does not appear in those cases.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.