Recipe schemas
Use a recipe schema to define a set of ingredients to create recipes.
A recipe defines values that correspond with the variables from the schema.
Recipes based on a recipe schema
TIP:
You can create multiple recipes based on a single recipe schema. It is useful for restoring previous recipe settings.
Provide Feedback