Add a sub-device
- In theFactoryTalk Remote Access Manager, access the section.
- In the domain left pane, select the primary device on which the sub-device is dependant.
- Next to the primary device, in its same line, select
. Alternatively, select the three dots at the top of the screen and select
Add subdevice. - ACreate Subdevicedialog window opens. Enter the sub-deviceNameandIP Address.NOTE: The sub-device IP address must be compatible with a subnet that is reachable by the remote device.
- SelectSave.
Provide Feedback