Sub-devices
Sub-devices may consist of devices such as PLCs, drives, iPCs, and similar, that are connected to a subnetwork and operate in conjuction with a remote device such as a Runtime, a router, or an HMI.
You can add one or more sub-devices for each remote device through the
Domain view
section in FactoryTalk Remote Access Manager
, and set any services for each sub-device. In this way, you can directly connect to the sub-device services without having to establish a VPN connection with the remote device first. When a connection establishes, an application opens based on the sub-device ip address.Provide Feedback